Options Dialog Box

The Options dialog box displays the following items:

Startup Profiles defined in this application override iFIX Startup command line parameters

Select this check box if you want the profiles created in this application to override the ones used when you start iFIX from the command line.  

For the override to work, the user must be defined in the Startup Profile Manager, or if the user is not defined, the default profile must be enabled.  

NOTE:  This override only applies to the /n, /s, and /l command line options.  

Nodename Prefix String

Enter the default iFIX node name prefix to use if the first 8 characters of the Windows user name cannot be used to generate a valid iFIX node name.

For each startup profile using the default iFIX node name, a number is also added to the end of the default node name, starting with the number 1.  For example, if the prefix is NODE, the default iFIX node names used are: NODE1, NODE2, NODE3, and so on.  

How Do I...