To change the
default settings for the Startup Profile Manager:
- In Classic view, in the iFIX WorkSpace, on the toolbar, click the Startup Profile Manager button.
-Or-
In Ribbon view, on the Applications tab, in the Utilities group, click Utilities, and then click Startup Profile Manager.
NOTE: The Startup Profile Manager can also be accessed from the Start menu by pointing to Programs, iFIX, Tools, and then Startup Profile Manager.
- On the Settings menu, click Options.
- Select the Startup Profiles defined in this application override iFIX Startup command line parameters check box, if you want the profiles created in this application to override the ones used when you start iFIX from the command line.
NOTE: For the override to work, the user must be defined in the Startup Profile Manager, or if the user is not defined, the default profile must be enabled. In addition, this override only applies to the /n, /s, and /l command line options.
- Enter the iFIX node name prefix that you want the Startup Profile Manager to use when the Windows user name is invalid as a default iFIX node name.
The Windows user name is an invalid iFIX node name, for instance, when the name starts with a number. Valid node names can be up to eight characters long. Node names can include alphanumeric characters, but must begin with a letter. Special characters, such as symbols and punctuation marks, cannot be used.
For each startup profile using the default iFIX node name, a number is also added to the end of the default node name, starting with the number 1. For example, if you enter NODE as the prefix, the default iFIX node names used are: NODE1, NODE2, NODE3, and so on.
- Click OK.