Working with Startup Profiles
iFIX must be running in order to use the Startup Profile Manager application. After you create your startup profiles and configure the default profile (if required), you need to save your startup profiles if you want iFIX to use them. If you do not save your startup profiles during the current session, a message box reminds you to save when you exit the Startup Profile Manager.
A startup profile is not used by iFIX until the specified user attempts to start iFIX from the iFIX Startup dialog box or from the iFIX Startup command line (from a desktop shortcut or the Run dialog box, for example). If no iFIX startup profile exists for the user and you do not define any settings in the Default User Profile dialog box or provide command line settings to the iFIX Startup application, when you restart iFIX, it displays the information from the last time iFIX was run.
See Also
Using the Startup Profile Manager
Startup Profile Manager Basics
Configuring the Options for the Startup Profile Manager
Configuring the Default Profile
Security Considerations when Using the Startup Profile Manager