Configuring the Default Profile
After configuring the application options for the Startup Profile Manager, you should define a default profile, if your iFIX configuration requires it. For instance, when using Terminal Services with the Startup Profile Manager, you will most likely want to configure a default profile.
If a user attempts to start iFIX and a profile does not exist for that user yet, iFIX starts with the default profile information.
To configure the SCU and iFIX Startup options for the default profile, use the Default Startup Profile dialog box, as shown in the following figure.
Default Startup Profile Dialog Box
Additionally, if iFIX is running as a service, you can configure the default SCU for the service, as illustrated in the previous graphic in the Default Service SCU area.
See Also
Using the Startup Profile Manager
Startup Profile Manager Basics
Configuring the Options for the Startup Profile Manager
Security Considerations when Using the Startup Profile Manager