Run-time Error Codes

If a network problem exists that prevents sessions from establishing or causes sessions to be terminated, one of the error codes listed in the following table may appear in the NETDIAG program.

Run-time Error Codes 

Error Code

Error Message

Description

1605

Command timed out.

These errors occur when the remote node is down. When the remote node is brought back up, the Connection Manager re-establishes the session.

1608

Invalid Local Session Number.

1610

Session Closed.

1624

Session Ended Abnormally.

1620

Can't find name called.

The session cannot be established because either a remote node is not operating, a cabling problem exists between the nodes, or the remote node name is not registered on the network. Verify both nodes are running compatible network software.

1914

Connection NOT established with node.

The Connection Manager has not yet established a connection with the remote node. Wait for Connection Manager to establish the session.

1960

FIX dynamic connection in progress.

Connection Manager is in the process of establishing a dynamic connection with the remote node. Wait for Connection Manager to establish the session.

1964

FIX has been shut down on remote node.

Connection Manager has detected that iFIX has been shutdown on the remote node. This error code shows up temporarily and then changes to 1914.

8517

Node not found in TCP hosts database.

The node name that you are trying to connect to be resolved to an IP address. The name is probably not in the local hosts file or on the WINS server. Obtain the remote node's IP address and add it to the HOSTS file.

 

See Also