You can enable network communications between any two iFIX servers by configuring each computer's network connections. To define these connections, click the Network button on the SCU toolbox.
You can use the Network Configuration dialog box to configure network protocols, configure network communications, establish dynamic connections. Refer to the following subsections for information on all of these functions.
- Configuring Protocols
- Configuring Remote Nodes
- Configuring LAN Redundancy
- Configuring Network Timers