Alarm Synchronization Tabbed Page Fields
The fields on the Alarm Synchronization tabbed page are described below.
Alarm Packets From Sync Queue – the number of alarm packets that were presented to the alarm acknowledgement synchronization task for processing.
Num Alarms Processed – the number of alarms that were processed by the alarm acknowledgement synchronization task. An alarm packet contains more than one alarm.
Num Alarms Failed Tag Resolution – the number of times the alarm acknowledgement synchronization task could not determine the tagname for an alarm.
Num Alarms Failed Local Status Read – the number of times the alarm acknowledgement synchronization task could not determine whether the local tag was already acknowledged.
Num Not In Alarm – the number of times the alarm acknowledgement synchronization task detected that the tag did not need to be acknowledged.
Num Alarms Failed Local Ack – the number of times the alarm acknowledgement synchronization task failed to acknowledge an alarm.
Num Alarms Acknowledged – the number of alarms acknowledged by the alarm acknowledgement synchronization task.