Alarm ODBC Tabbed Page Fields

The fields on the Alarm ODBC tabbed page are described below:

Database Id – the database ID as entered in the SCU.

Connection State – displays either CONNECTED to indicate a successful ODBC connection to the database, or LOST CONNECTION to indicate that the connection was not successful or was lost.

Table Name – the table name in the database as entered in the SCU.

Logging State – Displays either Active, indicating that alarms are taken from the queue and logged to the ODBC database, or Paused, indicating that alarms are taken from the queue and dropped (and thus are not logged to the ODBC database).

Reconnections – the number of times you needed to reconnect to the database.

Alarms Pending – the number of alarms in the user queue waiting to be processed.

Alarms Logged – the number of alarms successfully logged to the ODBC database.

 

See Also