Signal Select Block

Purpose

The Signal Select (SS) block provides a means of sampling up to six inputs, manipulating the inputs according to a user-selected mode, and sending the result to the next block.

Features

The Signal Select block:

  • Is a secondary block.
  • Supports changing the Selected Mode from a Data link, Program block, or Easy Database Access program.
  • Accepts multiple inputs and generates one output.

 

See Also

Typical Uses

Example

Fields