Signal Select Block – Modes

The Signal Select modes determine how the block handles its input values and calculates its output value. Each modes is described below:  

Alarm Type

Description

Average

Outputs the average of all assigned inputs. Bad or off scan inputs are not included in the calculation.

Good

Outputs the first input that FIX considers valid.

High

Outputs the highest input.

Low

Outputs the lowest input.

Sum

Outputs the sum of all the inputs. Bad or off scan inputs are not included in the calculation.

Inputs 1 - 6

Outputs the corresponding input number.