Selecting Commands Using the Multiple Command Script Wizard
To select one or more commands using
the Multiple Command Script Wizard:
- In the Basic Animation dialog box, click the Click button or select the Command check box. The Multiple Command Script Wizard appears.
- Choose a command from the Select Action to Append list. The Expert associated with the command you chose appears.
- Complete the Expert with your desired settings and information.
- Click OK. The Expert closes and appears in the Configured Actions list box of the Multiple Command Script Wizard.
- Optionally, repeat steps 2-4 if you want to add additional commands to your scripted command sequence.
- When you have finished choosing your command sequence, click OK to return to the Basic Animation dialog box.