Multiple Command Script Wizard Dialog Box
The Multiple Command Script Wizard lets you use one or more command Experts to build a sequence of actions that can be triggered by a mouse click on an object, a Scheduler entry, or a key macro.
The Multiple Command Script Wizard dialog box displays the following items:
Select Action to Append
The Select Action to Append drop-down list contains pre-defined Experts that you can add to your command sequence. When you select an action from the list, its associated Expert launches. After you configure the Expert for use in the sequence, it will appear in the Configured Actions list box.
NOTE: If the Expert you want to append is already displayed in the drop-down list, you can click the Append action button to launch the Expert.
Configured Actions
Append action button
Click this button to open the Expert currently displayed in the Select Action to Append list.
Delete a selected action button
Click this button to delete a selected action.
Delete all actions button
Click this button to delete all actions in the Configured Actions list box.
Up/Down buttons
Click the Up or Down button to move a selected action up or down in the Configured Actions list box.
Show/Hide action details button
Click the Show or Hide button to display or hide the details of all actions in the Configured Actions list box.
Modify selected action button
Click this button to modify the selected action.
Launch VB Editor
Click this button to launch the Visual Basic Editor.
Configured Actions List Box
The Configured Actions list box displays the command or sequence of commands that have been configured for the selected object. You can click the plus symbol next to a command to expand it and display its configured properties.