Exporting Enhanced Chart Dialog Box
The Exporting Enhanced Chart dialog box displays the following items:
Export
Item |
Description |
EMF |
Specifies EMF file format for chart export. |
WMF |
Specifies WMF file format for chart export. |
BMP |
Specifies BMP file format for chart export. |
JPG |
Specifies JPG file format for chart export. |
PNG |
Specifies PNG file format for chart export. |
Text/Data |
Specifies text/data file format for chart export. |
Export Destination
Item |
Description |
Clipboard |
Specifies that data is exported to the clipboard. |
File |
Specifies that data is exported to a file. |
Browse |
Click to choose a destination file and folder for export. |
Printer |
Specifies that data is sent to a printer. |
Export Size
Item |
Description |
|
Full Page |
Prints the exported chart on a full page. |
|
No Specific Size |
Specifies that no specific size is used for the exported chart. |
|
Pixel |
Specifies the unit of measure for the exported chart. This option is auto-selected for BMP, JPG and PNG file format and cannot be deselected. |
|
Millimeters |
Specifies that the size for the exported chart is measured in millimeters. |
|
Inches |
Specifies that the size for the exported chart is measured in inches. |
|
Points |
Specifies that the size for the exported chart is measured in points. |
|
Width |
Specifies the dimensions for the printed exported chart. NOTE: The width/height aspect ratio must be between .1 and 10.0 to avoid generating the error "This will produce an image that is hard to read. Please adjust output dimensions." For example, a width/height of 30/300 does not produce an error, but 30/301 does. Likewise, a width/height of 300/30 does not produce an error, but 301/30 does. |
|
The following fields are available only if Clipboard or File is selected in Export Destination. |
||
DPI |
Specifies the dots per inch. The higher the number the better the quality. |
|
Large Font |
Specifies a large size font is used in exported chart. |
Export
Click to export data to selected destination.