Exporting Enhanced Chart Data
To export enhanced
chart data:
- In the iFIX WorkSpace picture, double-click the chart. The Enhanced Chart Customization dialog box appears.
- Click Export.
- In the Export area, select the desired file format type.
- In the Export Destination area, select the desired export location. If you chose File, click Browse to set the destination.
- For Export options EMF, WMF, BMP, JPG, and PNG only, configure the export size. To do so:
- If applicable, select the unit of measure.
- Enter the export size in the Width fields.
NOTE: The width/height aspect ratio must be between .1 and 10.0 to avoid generating the error "This will produce an image that is hard to read. Please adjust output dimensions." For example, a width/height of 30/300 does not produce an error, but 30/301 does. Likewise, a width/height of 300/30 does not produce an error, but 301/30 does.
- Select the DPI.
- If desired, click Large Font.
- Click Export. If you selected the EMF, WMF, BMP, JPG, or PNG formats for export, your data is exported. Otherwise, the Exporting Enhanced Chart dialog box appears.
- On the Exporting Enhanced Chart dialog box, in the Export What area, select whether you want to export only the data or the data with its labels.
- In the Export Style area, choose to export the data in either list or table format. If you chose List, in the Delimited area, select either Tab or Comma. If you chose Table, in the Row vs Column area, select either Subsets/Points or Points/Subsets.
- In the Numeric Precision area, choose your level of precision.
- Click Export.