Using the Picture Pop-up Menu

When creating pictures, you can display a pop-up menu for that picture by right-clicking the picture name in the system tree, or by right-clicking any area in the picture outside of an object. The pop-up menu provides quick access to the picture's specific properties and animations, as well as common operations you can perform within the picture, such as selecting all objects.

The following table shows the functions that are available from the picture pop-up menu.

NOTE: Functions apply to both the Logical and Enhanced Coordinate Systems unless stated otherwise.

Picture Pop-Up Menu Functions 

Use the Operation...

To...

Animations

Display the Animations dialog box that lets you animate properties of the picture.

Undo

Cancel the previous operation. If a particular task cannot be undone, the Undo command is unavailable after you complete the action.

Paste

Place the most recently copied object into your picture.

Select All

Select all objects in the picture window.

Bring to Front

Move the selected picture to the front of the stack.

Send to Back

Move the selected picture to the back of the stack.

Space Evenly

Tile the open pictures in one of the following ways:

  • Horizontal
  • Vertical

Zoom

Change the width and height of the viewport by 50%, 150%, or 200% of the window size, or return the viewport size to 100% of the window size. The viewport is described in the Implementing Pictures in Your Process chapter.

Default View

Restore the original view of the picture before the window's size was changed.

NOTE: This function applies only to Logical Coordinate System pictures. This function does not apply to Enhanced Coordinate System pictures.

Full View

Expand the window to occupy the entire client-area.

NOTE: This function applies only to Logical Coordinate System pictures. This function does not apply to Enhanced Coordinate System pictures.

Fit Picture to Window

Resize the picture to fit inside the picture window, if necessary.

NOTE: This function applies only to Logical Coordinate System pictures. This function does not apply to Enhanced Coordinate System pictures.

Fit Window to Picture

Resize the window to fit the size of the picture, if necessary.

NOTE: This function applies only to Logical Coordinate System pictures. This function does not apply to Enhanced Coordinate System pictures.

Update Window Location

Preserve the current view of the picture so that, after being saved, it will look exactly the same way it did on the screen as when you closed it.

Refresh

Repaint the current picture in the picture window.

KeyMacros

Open the Key Macro Editor, which allows you to view and edit key macros.

Property Window

Display the Properties window for the current picture.

Picture

Display the Edit Picture dialog box, which allows you to change window properties.

Edit Script

Open the Visual Basic Editor, which allows you to edit Visual Basic scripts.

Enable Scripts

Reference all selected objects into Visual Basic scripts.

NOTE: The pop-up menu for pictures differs somewhat from the object pop-up menu. Refer to the Using the Object Pop-up Menu section for more information on the object pop-up menu.