Using the Tools Toolbar
Many of the advanced functions described in this section can be performed using the Tools toolbar. The following table shows you which functions are available and how they are used.
NOTE: Although hidden by default, you can access and use toolbars in Ribbon view. To access the Tools toolbar in Ribbon view, on the Home tab, in the WorkSpace group, click Settings, and then click Toolbars. You can also open a toolbar from the WorkSpace tree, by opening the Project Toolbar Files folder and double-clicking the toolbar you want to open.
By default, all of the buttons in the above table appear in the Toolbox. If you have the Toolbox enabled, click the button on the Toolbox.
Using the CAD Toolbar
The iFIX configuration environment provides a CAD (computer assisted drawing) toolbar with functions for manipulating line and polyline objects. The following table shows you which functions are available and how they are used.
|
||||
Click this button... |
Which can also be accessed in the Ribbon view... |
To... |
||
|
From the Format tab, in the Picture group, click Drawing Tools, and then click Extend Lines. |
Extend a selected line to intersect with another selected line. Refer to Extending Lines for more information. |
||
|
From the Format tab, in the Picture group, click Drawing Tools, and then click Trim Lines. |
Trim the selected lines to the intersection point. Refer to Trimming Lines for more information. |
||
|
From the Format tab, in the Picture group, click Drawing Tools, and then click Convert Lines to Polyline. |
Convert the selected lines to a polyline object. Refer to Converting Lines to Polyline for more information. |
||
|
From the Format tab, in the Picture group, click Drawing Tools, and then click Make Lines Horizontal. |
Change the selected line(s) to horizontal. Refer to Making Lines Horizontal or Vertical for more information. |
||
|
From the Format tab, in the Picture group, click Drawing Tools, and then click Make Lines Vertical. |
Change the selected line(s) to vertical. Refer to Making Lines Horizontal or Vertical for more information. |
||
|
From the Format tab, in the Picture group, click Drawing Tools, and then click Convert Line/Polyline to Pipe. |
Convert the selected line(s) or polyline(s) to a pipe object. Refer to Converting Lines and Polylines to Pipe for more information. |
||
|
From the Format tab, in the Styles group, click Pipe Styles, and then click Modify Pipe Characteristics. |
Open the Modify Pipe Characteristics dialog box for the selected pipes. Refer to Modifying Pipe Characteristics for more information. |
||
|
From the Format tab, in the Picture group, click Drawing Tools, and then click Add Connection Point. |
Add a connection point to anchor the selected connector to a shape. Refer to Adding and Deleting Connection Points for more information. |
||
|
From the Format tab, in the Picture group, click Drawing Tools, and then click Delete Connection Point. |
Delete a connection point anchor from the selected connector. Refer to Adding and Deleting Connection Points for more information. |
||
|
From the Format tab, in the Insert group, click Connectors, and then click Line Connector. |
Draw a connecting line between two shapes. Refer to Using the Connector Tools for more information. |
||
|
From the Format tab, in the Insert group, click Connectors, and then click Right Angle Line Connector. |
Draw a right angle connecting line between two shapes. Refer to Using the Connector Tools for more information. |
||
|
From the Format tab, in the Insert group, click Connectors, and then click Pipe Connector. |
Draw a connecting pipe between two shapes. Refer to Using the Connector Tools for more information. |
Using the Translation Toolbar
The iFIX configuration environment provides a translation toolbar with functions for exporting and importing language files. The following table shows you which functions are available and how they are used.
|
||
Click this button... |
To... |
|
|
Export the language file for the active picture. |
|
|
Export separate language files for one or more pictures. |
|
|
Import the translated language file for the active picture. |
NOTE: Translation functions are not available from the Ribbon in Ribbon view. To access these functions, you must display the Translation Toolbar. To access this toolbar in Ribbon view, on the Home tab, in the WorkSpace group, click Settings, and then click Toolbars. You can also open a toolbar from the WorkSpace tree, by opening the Project Toolbar Files folder and double-clicking the toolbar you want to open.
See Also
Grouping and Ungrouping Objects
Bringing to Front and Sending to Back
Trimming Lines at the Intersection
Making Lines Horizontal or Vertical
Converting Lines and Polylines to Pipe
How Do I...