The new pipe object inherits the property values, animation settings, and VBA scripts from the original line/polyline object. The pipe-specific properties have the default values configured in the User Preferences dialog box. You can change the pipe-specific properties using the Modify Pipe Characteristics dialog box.
The following diagrams show examples of converting lines and polylines to pipes.
Single Line Line Converted to Pipe |
Polyline Polyline Converted to Pipe |
See Also
Trimming Lines at the Intersection
Making Lines Horizontal or Vertical
Modifying Pipe Characteristics