Accessing the Create Picture Wizard

You can access the Create Picture wizard from the File menu (Classic View only), from the Ribbon (Ribbon view only), from the Task Wizard, and on several toolbars. The following table lists the most common ways to access the Create Picture wizard:

From the...

Do this...

Menu Bar
(Classic view only)

Select New from the File menu, then select Picture from the New list.

Ribbon
(Ribbon view only)

Click the WorkSpace button, select New, and then click Picture.

System Tree

Click the right mouse button on the Pictures folder in the System tree.

Task Wizard

Click the Task Wizard button from the Standard toolbar. Select Picture from the Task Categories list box. Select Create Picture Wizard from the Tasks list.

Experts Toolbar

Click the Create Picture Wizard button from the Experts toolbar.

Standard Toolbar

Click the Create Picture Wizard button from the Standard toolbar.

Toolbox

Click the Create Picture Wizard button from the Toolbox.

NOTE: To access the Create Picture wizard from the Menu Bar, the Ribbon, the System Tree, or the Standard toolbar, you must have the Show Picture Wizard from New Picture Menu check box enabled. You can enable this option in the Picture Preferences tab of the User Preferences dialog box.

Common Elements of the Create Picture Wizard

As you can see in the Introduction Page of the Create Picture Wizard, there are several elements of the Create Picture wizard that you will see on every page, including the following:

Preview Pane – Shows a picture configuration based on the currently selected options.

Help Button – Launches the Help topics for the Create Picture wizard.

Cancel Button – Exits the Create Picture wizard without creating any new pictures, or changing WorkSpace appearance.

Previous Button – Returns you to the previous page in the wizard.

Next Button – Sends you to the next page in the wizard.

Finish Button – Creates the new pictures that you have specified, and sets the WorkSpace appearance as you have specified. This button is only enabled when the wizard has enough information to successfully create new pictures.

See Also

How Do I...