Modify Configuration Dialog Box

You access the Modify Configuration dialog box from the Create Picture Wizard. The Modify Configuration dialog box displays the following items:

Attributes Tab

Item

Description

Show Title Bar

Adds a title bar to your picture.

Show System Menu

Adds system menus to your picture.

Resizable

Adds sizing borders to the picture.

Always on Top

Configures the window so that it is always on top when you open it.

Allow this Picture to be Cached

Configures the window so that when it is opened and closed it is held in memory and, when reopened, is read from memory.

Background Color

Click the Background Color button to set the actual background color of the picture. This color will not appear in the preview pane, since the colors in the preview pane are used only in the Create Picture Wizard.

Sizes Tab

Item

Description

Left

Distance from the left of the screen to the left edge of the picture.

Top

Distance from the top of the screen to the top edge of the picture.

Width

Distance from the left edge of the picture to the right edge of the picture.

Height

Distance from the top edge of the picture to the bottom edge of the picture.

Percentage Units

Indicates the size and location of the picture is based on percentage of the screen.

Pixel Units

Indicates the size and location of the picture is based on the number of pixels.

Help

Displays the Help for the current topic.

Save

Saves the changes for this picture only.

Save As

Saves the current options as a new configuration. When you select this option, the Enter New Configuration Name dialog box appears. Enter the name for the new configuration (up to 80 characters) in the Name field, then click OK to return to the Modify Configuration dialog box.

Return to Wizard

Closes the Modify Configuration dialog box and returns to the Create Picture Wizard.

How Do I...