Messages Appearing in AAM Tab of Mission Control
The following table details possible messages that the Auto Alarm Manager may display during its operation, and lists potential solutions to the problem that the messages convey. These messages appear in the top half of the AAM tab in the Mission Control window.
Message |
Solution |
Cannot find the phone book entry |
The primary or secondary contact specified in the SCU is not defined in the RAS phone book. Create a phone book entry for each contact before continuing. Refer to your Microsoft manuals for instructions. |
Hardware failure in port or attached device |
The Auto Alarm Manager cannot communicate with the local modem. Verify that the cable connection between the modem and the computer is secure. If the problem persists, try a different cable or modem. |
Cannot detect carrier |
The Auto Alarm Manager could not establish a connection to the Receiving node. Make sure the RAS server is running. Also make sure the local modem detects a dial tone when it dials the primary or secondary contact. |
ERROR_INTERACTIVE_MODE |
Do the following: 1. Select the phone book entry you want to edit. 2. From the Remote Access dialog box, click Edit. Click Advanced. If the Basic button appears, proceed to the next step. 3. Click Modem. 4. Clear the Enter Modem Commands Manually check box. 5. Close all open dialog boxes and exit the Remote Access program. The next time the Auto Alarm Manager dials, you should not receive an error. |
Testing the connection... |
After establishing RAS and iFIX connections, the Auto Alarm Manager on the Sending node sent a test message to the Receiving node and did not get a response. Make sure that Auto Alarm Manager is running on the Receiving node. If it is not, start it. |
The account does not have remote access permission |
The currently logged in user or the name of the user account specified in the Advanced Send Alarm Settings dialog box does not have the necessary rights to dial into the RAS server. Use the RAS Administrator program on the server node to grant dial-in rights to the necessary users. |
All AAM session attempts failed |
The Auto Alarm Manager could not communicate with the Auto Alarm Manager on the remote node. Make sure the following conditions exist:
|
Error 1311 setting emergency tag |
The Auto Alarm Manager could not set the specified Emergency tag configured in the SCU. Some of the reasons for this could be:
|
Error 1311 setting receive tag |
The Auto Alarm Manager could not set the specified Receive tag configured in the SCU. Some of the reasons for this could be:
|
Disable tag can't be read |
The Auto Alarm Manager could not read the specified Disable tag configured in the SCU. Some of the reasons for this could be:
If you get this error, the AAM will keep running, and it cannot be disabled. NOTES:
|