Name | Description | |
---|---|---|
![]() | Add | Add an archive to a Historian server. An archive may be newly created by the server or an existing, previously removed archive file. |
![]() | Backup | Request a backup of an archive from a Historian server. |
![]() | BackupConfig | Create a backup of the configuration. |
![]() | CloseCurrent | Close the current archive. Normally a Historian server automatically closes the current archive when it becomes full. This method allows manual control over the amount of data in the current archive. |
![]() | DropSubscriptions | Drop all the archive subscriptions. |
![]() | Get | Retrieve all properties for the archive of the given name. Archives are uniquely identified by name. |
![]() | GetStatistics | Retrieve archive statistics from a Historian server. |
![]() | Query | Retrieve a list of archives in a Historian server matching an archive name wildcard expression.
For large servers clients can optionally rely on large message sizes or result-paging or a combination of both to retrieve properties for a large number of archives. Maximum message size is straight-forward and controlled by ConnectionProperties.MaxReceivedMessageSize - it must be matched on both client and server. Result-paging enables large result sets to be retrieved across multiple server requests with timing and size controlled by the client. The number of results retrieved per request is controlled via the query's PageSize property. To utilize result-paging, specify a non-zero PageSize and continue calling the same query while the return code is true to retrieve all results from a server. To protect the server and limit excessive server-memory utilization initiating a second query without first retrieving all results for a first query generates a fault. |
![]() | Remove | Remove an archive from a server for off-line storage. The archive contents become unavailable for query. |
![]() | Set | Set the properties of an archive in a Historian server. Archives are uniquely identifed by name. |
![]() | SubscribeAny | Subscribe to archive changes in a Historian server such as: load, remove, modify or backup. Fires %% with details of the archive change. |
![]() | UnsubscribeAny | Clear any established archive subscriptions. |