Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / MaxReceivedMessageSize Property


In This Topic
    MaxReceivedMessageSize Property
    In This Topic
    Maximum size for a received message in bytes. Default is 1M.
    Syntax
    Public Property MaxReceivedMessageSize As System.Long
    public System.long MaxReceivedMessageSize {get; set;}
    public:
    property System.int64 MaxReceivedMessageSize {
       System.int64 get();
       void set (    System.int64 value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also