Data Store Configuration
Configure Data Stores
A data store is logical collection of tags used to store, organize, and manage tags according to the data source and storage requirements. A data store can have multiple archive files (*.IHA), and includes both logical and physical storage definitions.
Tags can be segregated into separate archives through the use of data stores. The primary use of data stores is to segregate tags by data collection intervals. For example, you can put a name plate or static tags where the value rarely changes into one data store, and your process tags into another data store. This can improve query performance.
Historian Data stores are stored archive files that contain data gathered from all data sources during a specific period of time. You can write and read data from the archives available under the data stores. Using data stores, you can store, organize, and manage tags according to the data source and storage requirements.
- Historical Data Store: Tags stored under historical data store will store data as long as disk space is available. Depending on your license, you may be able to create multiple historical data stores. The maximum number of Historical data stores supported depends on the license.
- SCADA Buffer Data Store: Tags stored under the SCADA buffer data store will store data for a specific duration of time based on license.
- System: Stores Historian messages and performance tags. This is only for internal usage within Historian, and you cannot add tags to this data store. You cannot rename or delete the System data store.
- User: Stores the data for the tags. This is a default data store. You can rename and delete a user data store as long as there is another default data store set for tag addition.
- SCADA Buffer: Stores short term tags and data in a SCADA Historian data store.
Adding a Data Store
About this task
Procedure
Renaming a Data Store
Procedure
Deleting a Data Store
About this task
Before deleting the data store, if there are any tags assigned to the data store, you must reassign these tags and manually move the data to another data store.
- You can only delete User data stores. You cannot delete the System data store. The Delete button will not be available, if you select a System data store.
- You cannot delete a data store if there are tags assigned to it. Reassign or delete the tags and then delete the data store.
- If you have only one User Store and System, you cannot delete the User Store.
To delete a data store
Procedure
Moving Tags Between Data Stores
About this task
To Move a tag between data stores
Procedure
Migrating Tag Data
When you move a tag from one data store to another, the incoming data for the moved tag, from that time on, will be stored under the new data store. The data residing in old data store can optionally be moved to the new store. This data cannot be retrieved unless it is moved to the new data store. You can move data using the Migration Tool. You can either move all the tags, or some tags. Before you migrate data, you have to back up the archive file(s) that contain the old data.
For more information, refer to Backing up an Archive Manually.
Migrating Tag Data using the IHA Migration Utility
To migrate tag data using the IHA Migration Utility, refer to the IHMigration Tool documentation. Ensure that you select the A Migration Tool section in the product IPI (Important Product Information). You can move all or some of the tags.