Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmInfo Class / DataSourceName Property


In This Topic
    DataSourceName Property (AlarmInfo)
    In This Topic
    Syntax
    Public Property DataSourceName As System.String
    public System.string DataSourceName {get; set;}
    public:
    property System.String^ DataSourceName {
       System.String^ get();
       void set (    System.String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also