Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmInfo Class / AlarmId Property


In This Topic
    AlarmId Property (AlarmInfo)
    In This Topic
    Syntax
    Public Property AlarmId As System.Integer
    public System.int AlarmId {get; set;}
    public:
    property System.int AlarmId {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also