Handling Value Step Changes with Collector Data Compression
Note: Individual tags can be configured to retrieve step value changes. Refer to the General Tab topic for more information.
If you enable collector compression, the collector does not send any new input values to the archiver if the value remains within its compression deadband. Occasionally, after several sample intervals inside the deadband, an input makes a rapid step change in value during a single sample interval. Since there have been no new data points recorded for several intervals, an additional sample is stored one interval before the step change with the last reported value to prevent this step change from being viewed as a slow ramp in value. This value marks the end of the steady-state, non-changing value period, and provides a data point from which to begin the step change in value. The collector uses an algorithm that views the size of the step change and the number of intervals since the last reported value to determine if a marker value is needed. The following is an example of the algorithm:BigDiff=abs(HI_EGU-LO_EGU)*(CompressionDeadbandPercent/(100.0*2.0))*4.0
If ( Collector Compression is Enabled )
If ( Elapsed time since LastReportedValue>=( SampleInterval * 5 ) )
If ( abs(CurrentValue-LastReportedValue) > BigDiff )
Write LastReportedValue,Timestamp=(CurrentTime-SampleInterval)
In the example above, if a new value was not reported for at least the last 4 sample intervals, and the new input value is at least 4 deltas away from the old value (where a single delta is equal to half of the compression deadband), then a marker value is written.Note: These settings are also adjustable from the Registry. Please contact technical support for more information.
Example: Value Spike with Collector Compression
A collector reads a value of X once per second, with a compression deadband of 1.0. If the value of X is 10.0 for a number of seconds starting at 0:00:00 and jumps to 20.0 at 0:00:10, the data samples read would be:
To increase efficiency, the straightforward compression would store only 2 of these 11 samples.
However, without the marker value, if this data were to be put into a chart, it would look like the data value ramped over 10 seconds from a value of 10.0 to 20.0, as shown in the following chart.

Time | X |
---|---|
0:00:00 | 10.0 (steady state value) |
0:00:01 | 10.0 |
0:00:02 | 10.0 |
0:00:03 | 10.0 |
0:00:04 | 10.0 |
0:00:05 | 10.0 |
0:00:06 | 10.0 |
0:00:07 | 10.0 |
0:00:08 | 10.0 |
0:00:09 | 10.0 |
0:00:10 | 20.0 (new value after step change) |
Time | X |
---|---|
0:00:00 | 10.0 (steady state value) |
0:00:10 | 20.0 (new value after step change) |
The addition of the marker value to the data being stored results in the following data values:
If you chart this data, the resulting trend accurately reflects the raw data and likely real world values during the time period as shown in the following chart.

Time | X |
---|---|
0:00:00 | 10.0 (steady state value) |
0:00:09 | 10.0 (inserted Marker value) |
0:00:10 | 20.0 (new value after step change) |