Historian Server Options
Allows you to set up your server information, limit or expand the application processing time, and input any needed security information. The Historian Server Options include:
Field | Description |
---|---|
Historian Server | The default server (set during installation). If you do not want to write data to the default server, enter the desired server in this field. |
Historian Username and Password | If you have created and established Security Groups in your Historian Security Environment, you may need to enter the user name and password here. By default, if you do not supply any information, the current logged in user will be used in security checking. For more information about Historian Security, refer to Implementing Historian Security chapter of the Getting Started manual. |
Event rate/sec | Allows you to limit the amount of server load caused by the Migration Utility. By reducing the Events/rate per second field in the Migration Options dialog box, you can allocate more time to real time collection. The default rate is 10,000. For more information, refer to Limit Processing Load on Server During Migration. |