Options Pane
Field | Description |
---|---|
Throttle Output | Select this option to throttle any part of the migration process. Optionally, you can remove this option as required. By default, throttling is rated at 5000 events per second. If you select this option, the migration might be a bit slow. |
Migrate Messages | Select this option to migrate the messages into the newly created archive. Using this option may or may not reduce the size of your archives, depending on the number of messages stored in the archive. By default, messages are migrated. |
Log File Full Name | Modify the location of the IHAMigration.log. |
Config File | The configuration (*.IHC) file that you want to migrate. You must provide the IHC file before selecting an IHA file. Do not specify an IHC file currently in use by the Data Archiver. Tip: It is always advisable to take a copy of the configuration file and work on the copy rather than working on the original file. |