Set Alarm Property Function

The Set Alarm Property function will set the value of the selected alarm property. It will take the inputs shown in the following table.

InputDescription
PropertySpecifies a property to get from the alarm object. If VendorAttribute is selected, additional list boxes will appear.
ValueSpecifies the property's new value.
AttributeSpecifies the vendor attribute to set. This list box will appear if you have selected VendorAttribute in the Property list box.
Value TypeSpecifies the data type for the vendor attribute. Valid data types are:
  • Numeric
  • String
  • Time
Note: The Set Alarm Property function will not automatically save changes to the alarm object. To save changes to the alarm object, you must use the Update Alarm function.