Data Stores Page
The Data Store Information page lets you read, add, rename, and delete the data stores. To view the Data Stores, click the Configuration link, and then click the Data Stores link. The Data Stores page appears and displays the list of available data stores and their details. For more information, refer to the Configure Data Stores section.
The following table describes the fields available in the Data Stores page:
Field | Description |
---|---|
Data Store Name | Displays the name of the data store. |
Type | Indicates whether the storage type is Historical or SCADA buffer. |
Description | Displays the description of the data store. |
Is Default | Indicates whether the data store is the default store. Select Yes if you want to set the data store as the default data store. |
Number of Tags | Displays the number of tags the data store contains. |
State | The state that the data store is in. The data store state is always running until you delete the data store. |
Edit | Click this button to edit the data store configuration. |
Delete | Click this button to delete the data store. |
Details | Click this button to view the archive details of the data store. |