Setting Up the Historian OPC HDA Server
About this task
Setting up and using Historian OPC HDA Server involves the following steps:
Procedure
- Install the Historian OPC HDA Server. For more details, refer to the Installing the Historian HDA Server section.
- Start the Historian Non-Web Administrator.Note:
You must install Historian Non-Web Administrator in order to set up the OPC HDA Server.
- Open the Historian Administrator Login dialog box. If Historian is already open, double-click the Main button to open the Historian Administrator Login dialog box.
- Click Browse for Server.
- From the Servers list, select the Historian server to configure .
- Click Set Selected Server as Target of HDA Server, and then click OK.
The selected server is set as the target Historian server.
Note: You must disconnect and reconnect all HDA clients before connecting to Historian OPC HDA Server. - Configure any external OPC HDA Clients to connect to the Historian HDA Server. The Proficy OPC HDA Server uses Proficy.Historian.HDA as the ProgID (Program ID).