Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Installing Cygnet Collector
About this task
The Cygnet Data Collector consists of System API as well as the Collector Toolkit components.
Before you begin
Installation Prerequisites The following must be installed on the system before the Cygnet Collector can be started:
Cygnet 64 Bit API (installed and registered)
Cygnet 64 Bit ODBC Driver
The following error is reported by the collector, if the Cygnet 64 Bit APIs are not installed:
Error Setting Cygnet GlobalFunctions object: 'Class not registered'
Follow the step below to manually install the CxScript64.dllrequired by Cygnet Collector: regsvr32 "C:\...\8.1.2 Install\Cygnet 812\Support64\CxScript64.dll"
Note: The install location of the CxScript64.dll file may differ from that specified above.
Installing Cygnet Collector via the installer
Note: The Cygnet Collector Service must be setup to run from an account that has access to the Cygnet system.
On the Historian installer wizard, select Cygnet collector option.
Click Next.
Click Finish at the end of the wizard to install Cygnet Collector.
Uninstalling Cygnet Collector
To uninstall Cygnet Collector installed via the installer, go to Add/Remove programs, select Historian Collectors and click Uninstall.
Note: Be informed that this will uninstall any other collector installed on your computer!
Installing Cygnet Collector manually
To install multiple instances of Cygnet collector manually through a command line interface:
Procedure
Copy ihCygnetCollector.exe to the right folder:
If the Historian Data Archiver is installed, then the path is: C:\Program Files\Proficy\Proficy Historian\x64\Server .
Start a command prompt and Run it as an administrator.
From the command prompt, register the service:
Note:binPath will depend on the installation. See step 1 above.
Verify if the Historian Cygnet Collector is visible in the service control.
From the Services panel do the following:
Set the Startup type to Automatic.
Set the Log on as property to use a system account that has rights to read from the Cygnet application.
Create a key with the registry name used, for example, "Cygnet_01".
Run the regeditcommand to open the Registry Editor. Navigate to: HKEY_LOCAL_MACHINE\SOFTWARE\GE Digital\Historian Cygnet Collector\iHistorian\Services\CygnetCollector\.
Right click on CygnetCollector and Create key called Cygnet_01.
Create the following registry entries with String value type.
Modify the following Keysas needed:
HistorianNodeName - Name of Proficy Historian where the collector sends the data.
InterfaceName - Name of the collector as it will be identified in the Proficy Historian Archiver (must be unique). The interface name must include Cygnet(Eg: CygnetCollector, MyCygnetCollector, TestCygnet are all acceptable)
ServiceSite - This must be populated with the correct Cygnet site before re-starting the collector.
Start the Cygnet Collector to create the full set of registry key. The Service should continue to run if you have configured the above keys properly and have access to the Cygnet services.
What to do next
Uninstalling manually installed Cygnet Collector
To uninstall\delete the multiple instances of Cygnet collector installed manually from command line running as admin:
sc getkeyname to get the proper key for deletion.
sc delete <keyname>
For example: sc getkeyname Historian Cygnet Collector[SC] GetServiceKeyName SUCCESS Name = IHCygnetOne sc delete "IHCygnetOne[SC] DeleteService SUCCESS
Note: A machine reboot may be required for the removal of service and registry entries to take affect.