Using the UAA Config Tool
About this task
- Add a local UAA user.
Here a local UAA user means a user defined by UAA, not by an external identity provider such as LDAP.
- Remove a local UAA user.
- Reset the password for a local UAA user.
- Add a local UAA user to an existing UAA group.
Since OAuth2 scopes are implemented as UAA groups, this means the same as adding a scope to a user.
- Remove a local UAA user from an existing UAA group.
A user who performs these functions is acting as the adminclient and needs to know the secret of the admin client. The tool does provide a way for the user to cache the secret safely to be used later.
The tool is installed in the UAA subdirectory of the Historian installation directory, typically C:\Program Files\GE Digital\UAA. Run the tool from a Windows command prompt window.
Syntax
The tools syntax follows this format:
uaa_config_tool verb [options]
add_user
remove_user
set_user_password
add_user_to_group
remove_user_from_group
clear_secret
Run the tool without a verb or any other options to view the help screen.
Options can be specified in the form of single dash followed by a short name, or double dash followed by a long name, followed by the value of the option, if any. For example, you can specify the user name Alice
by either
-u Alice
or
--UserName Alice
Options
Short name | Long name | Remark |
-t | --Target | URL of the UAA instance that the command should be performed on. Typically, the URL is https://localhost:8443/uaa, which is the default value. This option is optional and is only needed when the user wants to run the command against a remote UAA instance (which is not recommended due to security concerns). |
-n | --ClientId | ID of the client that the user is acting as. By default, it is admin . This option is optional and is only needed when the admin has set up the UAA to delegate certain operations to others. |
-s | --ClientSecret | This is the secret used to authenticate the user for acting as the admin client (or an alternative client given in a --ClientId option). If the user has elected to cache the secret previously, then this option can be omitted. Otherwise, it has to be provided. |
-c | --CacheSecret | This option is not followed by a value and is optional. If specified, the tool will cache the client secret so when the next time this tool is invoked the secret does not have to be specified. Note that the secret is encrypted and only the current Windows logon user can access and decrypt. |
-u | --UserName | Name of the user that the tool is being invoked for. For example, the user that is being added or removed. |
-p | --UserPassword | The password for the user being added or whose password is being reset. The option is only needed for the add_user and set_user_password commands. |
-g | --Group | Name of the UAA group (scope) that the user is being added to or removed from. The option is only needed for the add_user_to_group and remove_user_from_group commands. |
Examples
- To add a new user named
bob
with the passwordbobcat2
(with the admin client secretMyNotSoSecret
specified on the command line, to be cached and used later):uaa_config_tool add_user -u bob -p bobcat2 -s MyNotSoSecret -c
- To add user
bob
to the grouphistorian_visualization.user
, using the previously cached admin secret:uaa_config_tool add_user_to_group -u bob -g historian_visualization.user
- To remove user
alice
from a remote instance of UAA as an alternative client (that is, other thanadmin
)useradmin
:uaa_config_tool remove_user -u alice -t https://webhost.lab:8443/uaa -n useradmin -s MyOtherNonSecret
- To clear any cached client secret:
uaa_config_tool clear_secret
Note: If the Windows logon account is not shared, it is not necessary to clear cached secret, since the cache is encrypted and only the same Windows user account can decrypt.