About this task
The ODBC Collector supports auto-reconnect to the ODBC Server. If the connectivity between the ODBC server and the collector is down due to network connectivity issues, the collector will auto-reconnect to the server when the server is back and running. The collector polls for the server connection for a set time of every 5 seconds. The collector shuts down when the reconnect functionality is disabled.To enable Auto-Reconnect to the ODBC Server:
Procedure
- From the Start menu, click Run and type Regedit, then, click OK.
The Registry Editor appears.
- Open the key folder: HKEY_LOCAL_MACHINE\SOFTWARE\GE Digital\iHistorian\Services\ ODBCCollector.
- Create a new DWORD labelled, EnableReconnect.
- Enter the decimal value 1.
- Click OK, then close the Registry Editor.
- Restart the ODBC Collector for the change to take effect.
Important: If this registry is not created and set to a value of 1, then the auto-reconnect functionality will not be enabled.
To configure the timer: - From the Start menu, click Run and type Regedit. Then, click OK. The Registry Editor appears.
- Open the key folder: HKEY_LOCAL_MACHINE\SOFTWARE\GE Digital\iHistorian\Services\ ODBCCollector.
- Create a new DWORD labelled, ReconnectInterval.
- Enter a decimal value greater than 5. This value represents the number of seconds for the collector to wait before trying to re-connect to the ODBC Server.
- Click OK, and then edit the Registry Editor. Min Value = 5 seconds (default) Max Value = 60 seconds
- Click OK, and then edit the Registry Editor.
- Restart the ODBC for the change to take effect.