WHERE Clauses
The Historian OLE DB Provider supports the use of WHERE
clauses to specify search conditions in a SELECT
statement. You can specify a condition for any column in the table using the WHERE
clause.
For example, you could use a simple WHERE
clause to search all rows of data in the ihTags table, where the DataType
column equals SingleFloat
. In another instance, you might want to find all tags that belong to a particular collector. Or, you might also want to search for all tags with a certain poll rate, or range of poll rates, or ones with polling disabled.
For more information on the columns for each individual Historian table, see Historian Database Tables.
SELECT
statement.Example 1: Search for All Single Float Tags
SELECT* FROM ihtags WHERE datatype=singlefloat
Example 2: Specify Query Parameters to Obtain String Data
In the following example, you change the SamplingMode
column from the default value of Calculated
to Interpolated
in order to retrieve string data.
SELECT* FROM ihrawdata WHERE tagname=SimulationString00001
AND samplingmode=interpolated
AND IntervalMilliseconds=1H
Example 3: Use a WHERE Clause to Specify a Time Range
SELECT* FROM ihmessages WHERE timestamp>bom
Example 4: Use a Complex WHERE Clause to Find All Tags With a Specific Name and Description Pattern
SELECT* FROM ihtags
WHERE(tagname LIKE '*001*' AND description LIKE '*sim*')
OR (tagname LIKE '*02*'
AND (description LIKE '*sec*' OR description LIKE '*sim*'))
AND (timestamptype=source OR timestamptype=collector)
For more information on building complex WHERE
clauses, see Logical Operators and Parenthetical Expressions.