Alerts Panel

The Alerts panel displays all alerts and warnings received or generated by the system. You can scan through these messages by using the scroll bar at the right of the window. It displays the system timestamps and records of each message in this window. Both of the below are tasks and should be in task type topics.

To stop automatic updating of the display in the Historian Non-Web Administrator, clear the Show Alerts check box. This setting will be reset when you restart the Non-Web Administrator.

To automatically refresh the alerts panel statistics, select Auto option in the Alerts panel. Selecting the Auto option automatically refreshes the last five seconds alerts panel statistics every 25 seconds. You can also click the Refresh button on the alerts panel to manually refresh the alerts panel statistics.

TheSystem Statistics > Alerts panel screen displays data described in the following table.

Table 1. Alerts System Statistics
FieldDescription
TimestampThe timestamp associated with the message or alert.
TopicThe type of alert message. Only the Services and Performance alerts appear here. A total of up to 250 of the most recent messages will be displayed.
MessageThe content of the message or alert.