Interpolated Data API

The Interpolated Data API queries interpolated values for a list of tags. If the start time equals the end time, the request returns one sample.

METHOD:GET, POST
URI:
GET
https://<historianservername>:8443/historian-rest-api/v1/datapoints/interpolated/{tagNames}/{start}/{end}/{count}/{intervalMs}
POST
https://<historianservername>:8443/historian-rest-api/v1/datapoints/interpolated/{start}/{end}/{count}/{intervalMs}
SAMPLE GET URI:https://<historianservername>:8443/historian-rest-api/v1/datapoints/interpolated/tagName1/2013-10-02T11:30:00.111111Z/2013-10-02T11:31:11.111Z/100/10000
SAMPLE POST URI:https://<historianservername>:8443/historian-rest-api/v1/datapoints/interpolated/2013-10-02T11:30:00.111111Z/2013-10-02T11:31:11.111Z/100/10000
SAMPLE cURL COMMAND (GET):curl -i -H "Accept: application/json" -H "Authorization: Bearer <TOKEN>http://<nodename>:8443/ historian-rest-api/v1/ datapoints/interpolated/<tagName>/<start time>/<end time>/<count>/<intervalMS>
SAMPLE cURL COMMAND (POST):curl -i X POST -H "Content-Type: application/json" -H "Accept: application/json" -H "Authorization: Bearer <TOKEN>-d {\tagNames\:\<tagName>\}http://<nodename>:8443/ historian-rest-api/v1/ datapoints/interpolated/<start time>/<end time>/<count>/<intervalMS>

Query Parameters

ParameterDescriptionRequired?Values
TagNameQueries the tag names specified.YesString
StartStart time of the query, in ISO data format (such as YYYY-MM-DDTHH:mm:ss.SSSZ).YesDateTime
EndEnd time of the query, in ISO data format (such as YYYY-MM-DDTHH:mm:ss.SSSZ).YesDateTime
CountCount of archive values within each calculation interval.YesInteger, with a value such as 100.
intervalMSInterval in milliseconds.Yes64-bit signed integer, with a value such as 10000.

Response Parameters

ParameterData TypeRequired?Description
ErrorCodeIntegerYesFor example, 0.
ErrorMessageStringYesFor example, NULL.
DataStringYesThe object container for the following parameters:
DataType
DoubleFloat, which stores decimal values up to 15 places.
ErrorCode
Value is 0, which means the operation was successful.
TagName
Example is TagName1.
Samples
Provides TimeStamp, Value and Quality for each sample. For example, TimeStamp = 2013-10-02T11:30:00.111Z, Value = 34.26155, and Quality = 3.

Sample Response

{
     "ErrorCode" : 0,
     "ErrorMessage": null,
     "Data":[{
      "DataType":"DoubleFloat",
      "ErrorCode":0,
      "TagName":"TagName1",
      "Samples":[ { "TimeStamp":"2013-10-02T11:30:00.111Z","Value":"34.26155","Quality":3 },
                  {  "TimeStamp":"2013-10-02T11:30:10.111Z", "Value":"37.26155", "Quality":3  }, 
                                        
                  {  "TimeStamp":"2013-10-02T11:31:00.111Z", "Value":"33.26155", "Quality":3  }                 
                ]
     }]
}