ihAlarms Table
The ihAlarms table contains collected alarm and event data. The following table describes the columns of the ihAlarms table.
CAUTION: When you perform joins of the ihRawData and ihAlarms tables, you can easily construct queries that temporarily consume all your system resources. Although this scenario typically does not affect data collection, it can interfere with data analysis. To avoid this issue, always define a start and end time for the query to limit the number of rows returned.
Column Name | Data Type | Description |
---|---|---|
AlarmID | VT_I4 | The unique ID of the alarm or event in the Historian alarm database. |
ItemID | VT_BSTR | The OPC ItemID of the alarm. This contains the source address of the data access tag with which the alarm is associated. This can contain a NULL value if an alarm is not associated with a tag. |
Source | VT_BSTR | The unique identifier used by the OPC AE Collector for the alarm or event. |
DataSource | VT_BSTR | The collector interface name associated with the alarm or event. |
Tagname | VT_BSTR | The Historian tag name associated with the alarm. This value is NULL unless the tag is also collected by Historian. |
AlarmType | VT_BSTR | The alarm type:
|
EventCategory | VT_BSTR | The OPC event category of the alarm or event. |
Condition | VT_BSTR | The OPC condition of the alarm. Does not apply to event data. This value combined with the Source value comprises an alarm. |
SubCondition | VT_BSTR | The OPC subcondition of the alarm. Does not apply to event data. This value represents the state of the alarm. |
StartTime | VT_DBTimeStamp | The start time or timestamp of the alarm or event. |
EndTime | VT_DBTimeStamp | The end time of the alarm. Does not apply to event data. |
AckTime | VT_DBTimeStamp | The time the alarm was acknowledged. Does not apply to event data. |
Microseconds | VT_I4 | The microsecond portion of the date and time. |
Message | VT_BSTR | The message attached to the alarm or event. |
Acked | VT_BOOL | Stores the acknowledgement status of the alarm. If the alarm is acknowledged, this is set to TRUE . |
Severity | VT_I4 | The severity of the alarm or event. Stored as an integer value with a range of 11000. |
Actor | VT_BSTR | The operator who acknowledged the alarm, or caused the tracking event. |
Quality | VT_VARIANT | The quality of the alarm or event. Stored as a string, with values of GOOD or BAD . |
TimeZone | VT_BSTR |
The type of time zone used:
|
DaylightSavingTime | VT_BOOL | Indicates whether Daylight Saving Time logic should be applied to timestamps. |
RowCount | VT_I4 | The maximum number of rows returned by the current query. |
User-Defined Variable #X | VT_VARIANT | User-defined variables. This is a dynamic list of columns that varies based on the collectors running on the Historian system. |
Note: Additional fields may be added by third-party products such as iFIX. Please consult the relevant product documentation for further information.
ihAlarms Examples
Example 1: Show All Alarms for the Last Two Hours, Including Vendor Attributes
SELECT * FROM ihAlarms
SELECT * FROM ihAlarms WHERE alarmtype = alarms //same as above
Example 2: Show Alarm History
SELECT * FROM ihAlarms WHERE alarmtype = alarm_history
Example 3: Show Tracking and System Events
SELECT * FROM ihAlarms WHERE alarmtype = events
Example 4: Return All Closed Events and Associated Tag Data
SELECT
alarmid, ihalarms.tagname, ihalarms.starttime, ihalarms.endTime, ihrawdata.timestamp, ihrawdata.value
FROM ihalarms, ihrawdata
WHERE ihalarms.tagname=ihrawdata.tagname
AND ihalarms.starttime <= ihrawdata.timestamp
AND ihalarms.endtime >= ihRawdata.timestamp
AND ihalarms.subcondition == "OK"
OR ihalarms.quality = "Bad"
ORDER BY ihalarms.starttime
Note: When you join data from the ihRawData and ihAlarms tables, be sure to specify a timestamp range.
Example 5: Return All Open Alarms and Associated Tag Data
SELECT
alarmid, ihalarms.tagname, ihalarms.starttime, ihalarms.endTime, ihrawdata.timestamp, ihrawdata.value
FROM ihalarms, ihrawdata
WHERE ihalarms.tagname=ihrawdata.tagname
AND ihalarms.starttime <= ihrawdata.timestamp
AND ihalarms.endtime >= ihRawdata.timestamp
AND ihalarms.subcondition <> "OK"
AND ihalarms.quality = "Good"
ORDER BY ihalarms.starttime
Note: When you join data from the ihRawData and ihAlarms tables, be sure to specify a timestamp range.