Current Value Table Description
The required elements for the Current Value Table are described in the following table.
Number | Component | Description |
---|---|---|
![]() | Title | Allows you to enter a name for your Current Value Table. By default, the title is automatically labeled Current Value 1, Current Value 2, Current Value 3, and so forth until you change it. |
![]() | Remove Selected | Deletes the selected tag from the Current Value Table. |
![]() | Filter | Type any text to dynamically and quickly filter your view based on desired criteria. This impacts all columns. |
![]() | Name | Lists the Historian tag name of the tags you selected in the Current Value Table. |
![]() | Time | Contains the time stamp from Historian based on a current value query, meaning that it is the most current value and its time stamp based on what is in the Historian. |
![]() | Value | Lists the most current value in Historian for the selected tag. |
![]() | Quality | Indicates the quality of the tag (Good or Bad) as it receives it from Historian. |
![]() | Units | Lists the EGU Description for the tag as captured in Historian. |
![]() | Description | Lists the Description for the tag as captured in Historian. |
![]() | Display Number | Lets you select the number of entries to display without pagination in the Current Value Table (maximum of 7). |
![]() | Page Selector | Allows you to select which page to display when there is more than one page available. |