Can I Retrieve Data From Multiple Servers?
Yes. The OLE DB Provider can have connections to multiple servers at the same time. Each is regarded as a separate session.
You cannot mix multiple servers in the same SELECT
statement, except indirectly in a linked server in Microsoft SQL Server. Crystal Reports allows you to create subreports inside of a report. Each report gets its own data source (which would be a Historian server) and its own SELECT
query. However, the reports cannot share data. You can have multiple VisiconX data controls in one picture, each going to a different server.
For instance, say you run iFIX and Crystal Reports at the same time. From the VisiconX screen, establish a connection to the Historian OLE DB Provider and perform a query on Server1. Next, run a report from Crystal Reports connecting to the same provider, but with a connection to a different server, Server2. After you run the report and go back to the VisiconX screen, you will notice that VisiconX is still connected to Server1. If you refresh the control, it uses the same settings and server as it did before. The provider maintains these two sessions separately, each with its own SET
parameters.
So, in general, you can access multiple servers, but the data from each server remains independent. You must work with linked servers in Microsoft SQL Server to combine data from multiple servers.