System API Connect Functions
Not every function and structure in the ihapi.h
is documented or available for use in user written pro- grams. Please limit your programs to the documented functions or contact the Technical Support team at GE Intelligent Platforms for additional clarifications.
Connect Functions
To perform a connection you need to just use the connect functions. The API will complete the connection and do further necessary reconnects when the Data Archiver is restarted. Your program does not need to manage and monitor connections as it is done by the API.
Connections are subjected to Historian security, which is based on Microsoft Windows Security.
It is expected that user written programs will connect a minimal number of times for staying connected and using that connection for all read and write calls. Connecting and disconnecting rapidly is not efficient. The connect functions are:
ihServerConnect
ihServerConnect(
ihString ServerName,// the computer name or IP address of the Machine running the Data Archiver. You can pass
NULL or the empty string ”to attempt connection to a Data Archiver on your local machine.
ihString Username,// The windows username to use when connecting or NULL if you want to connect as the process
owner of your program, typically the logged in user. You would specify a username if the process owner was unable to
connect or did not have sufficient Historian Security permissions.
ihString Password,// if you passed a Username you can pass the password or ”if there is no password or
otherwise just pass NULL
ihString BufferFileName, // an optional bufferfilename if your program will be using store and forward to
deliver written data
ihServerHandle *hServer // this is an output parameter that will contain the server handle that you would use in
later read and write calls
);
Remarks
A server is a computer running a Data Archiver. You can specify a server by including the computer name or IP address.
ihServerConnect()
will initiate a connection, but you should really use
ihServerIsConnected()
to determine if the connect actually completed.
If you setup a connection callback function with ihServerRegisterConnectionCallback()
you will be notified of connection changes. Your security permissions for reads and writes will be established at connect time and are based on the user name and password provided.
Returns
Returns Status | Message |
---|---|
ihSTATUS_OK | On success. |
ihSTATUS_API_TIMEOUT | If the server name or IP address provided cannot be located. |
ihSTATUS_LIC_TOO_MANY_USERS | If this connection would exceed your licensed number of connections. |
ihSTATUS_NOT_VALID_USER | If the user is not allowed to connect. This can happen whether you provided a username or connected as the process owner. Consult the Historian documentation for security behavior. |
ihSTATUS_FAILED | For any other type of error. |
ihServerDisconnect
Use this function to disconnect from the Historian server.
ihSeverDisconnect {
ihServerHandle hServer // the handle returned by a previous call to ihServerConnect
);
Remarks
You should call ihServerDisconnect()
function even if the connection attempt returned an error.
Returns
Returns Status | Message |
---|---|
ihSTATUS_OK | On success. |
ihServerIsConnected
This function returns whether the Historian server is currently connected or not. It is an indication that if you try to read and write data the call should be successful.
Prototype
ihServerIsConnected {
ihServerHandle hServer // a server handle returned from ihServerConnect
};
Returns
Returns Status | Message |
---|---|
ihSTATUS_OK | On success. |
ihSTATUS_FAILED | On failure. |
ihServerSetTimeout
This function is used to configure the timeout of the server connection.
Prototype
TihServerSetTimeout {
ihServerHandle hServer, // a server handle returned from ihServerConnect
int Timeout // the timeout, in seconds, to use
};
Use this to configure the timeout to a larger or smaller value. If the System API does not receive any response, even a partial response, during the timeout value, a ihSTATUS_API_TIMEOUT
will be returned from the API call.
Set the timeout any time after connecting and the timeout stays in effect until it is changed or disconnect is issued.
Returns
Returns Status | Message |
---|---|
TRUE |
if you are currently successfully connected. |
FALSE
|
if you were never connected or if the connection is currently down and being re-established. |
ihServerGetTimeout
ihServerGetTimeout {
ihServerHandle hServer, ihULong *timeout
};
Remarks
Call ihServerConnect()
to make a connection, then ihServerSetTimeout()
to set the timeout if you want a non default value. You can use the ihServerGetTimeout()
function to determine the timeout value that is being used.
The returned timeout value is in seconds.
Returns
Returns Status | Message |
---|---|
ihSTATUS_OK | On success |
ihSTATUS_FAILED | On failure |
ihServerGetVersion
This function returns the Historian server version and connection status.
Prototype
ihServerGetVersion {
ihServerHandle hServer, // a serverhandle returned from a previous call to ihServerConnect
int *Major, // output parameter to contain the major version of the Data Archiver.
For example 4 when the Data Archiver version is 4.5.
int *Minor, // output parameter to contain the minor version of the Data Archiver.
For example 5 when the Data Archiver version is 4.5.
int *Build, // output parameter to contain the build number of the Data Archiver. This is typically not used.
int *Revision // output parameter to contain the revision number of the Data Archiver. This is typically not used
};
You will not receive an immediate callback with the current connection status. You will be notified of the next change in status
Remarks
You will not receive an immediate callback with the current connection status. You will be notified of the next change in status.
Returns
Returns Status | Message |
---|---|
ihSTATUS_OK | On success and the desired information can be read from the output parameters. |
ihSTATUS_FAILED | On failure. |
ihSecurityGetMembership
This function returns your membership list. Your group memberships determine your security permissions and what calls you can make on this Proficy Historian server connection.
Prototype
ihSecurityGetMembership {
ihServerHandle hServer, // handle from previous call to ihServerConnect
ihSecurityGrpMembership *Memberships // output parameter to contain the group membership list
};
Remarks
You can optionally use this call after a successful connect to determine whether the Data Archiver considers your membership list. You need to be completely connected, not just initiate a connection, before this call can be used. The best way is to use ihServerIsConnected()
after
ihServerConnect()
to determine that the connection completed.
Returns
Returns Status | Message |
---|---|
ihSTATUS_OK | On success and the desired information can be read from the output parameter. |
ihSTATUS_API_TIMEOUT | If the call could not be completed. |
ihSTATUS_NOT_CONNECTED | When not currently connected to the Data Archiver. |
ihSTATUS_FAILED | When the other three return options otherwise do not apply. |
ihServerOpenRecordset
This function returns the list of Historian servers that exist in the Windows registry.
Prototype
ihServerOpenRecordset {
ihString ServerNameMask, // typically NULL to get all servers but could be a mask
ihServerRecordset *ServerRecordset // output parameter containing the recordset
};
Remarks
Use this function to get the list of servers that exist in the Registry. This is a local call and does not need the Data Archiver.
The default server is stored in the Registry and can be used to query instead of hardcoding a server name in your program or prompting the user. The default server is established during product install and can be changed anytime later
Returns
Returns Status | Message |
---|---|
ihSTATUS_OK | On success and the desired information can be read from the output parameter. |
ihSTATUS_FAILED | On failure |
ihServerCloseRecordset
This function is used to free any memory such as server names that were allocated in the System API.
Prototype
void ihServerCloseRecordset {
ihServerRecordset *ServerRecordset // recordset returned from ihServerOpenRecordset
};
Use this function to free any memory such as server names that were allocated in the System API in the ihServerOpenRecordset()
call.
Returns
void