INCLUDEBAD
The INCLUDEBAD modifier directs the Data Archiver to consider raw samples of bad data quality when computing calculation modes. Use INCLUDEBAD modifier to consider both good and bad quality values.
You can use the INCLUDEBAD modifier with any Sampling or Calculation mode only if you want to include bad quality data.
Use the INCLUDEBAD modifier only if you believe the bad quality data has meaningful values and are useful as input to calculations. Most bad data quality values do not have meaningful values; they show 0 or unpredictable numbers. But in some cases, if the data is being written using a user program instead of a collector, you can use this query modifier.
Bad data always has a sub quality such as Comm Error or Configuration Error. When you use the INCLUDEBAD modifier any end of collection raw samples or calculation error raw samples are still ignored because they are not process data, just data markers that are inserted by collectors.
- Example
-
Import this data to demonstrate the behavior of the INCLUDEBAD query modifier:
[Tags] Tagname,DataType,HiEngineeringUnits,LoEngineeringUnits Tag1,SingleFloat,60,0 [Data] Tagname,TimeStamp,Value,DataQuality Tag1,07-05-2011 17:24:00,29.72,Bad Tag1,07-05-2011 17:25:00,29.6,Good Tag1,07-05-2011 17:26:00,29.55,Good Tag1,07-05-2011 17:27:00,29.49,Bad Tag1,07-05-2011 17:28:00,29.53,Bad
Note: The given sample contains three bad quality data.Run the following query
set starttime='07-05-2011 16:00:00', endtime='07-05-2011 21:00:00' select timestamp,value,quality from ihrawdata where tagname like 'Tag1' and samplingMode=calculated and CalculationMode=count and Numberofsamples=1
Time Stamp Value Quality 7/5/201121:00:00 2.000000000000 100.0000000 The count is 2 because only good quality data is considered. If you want to consider bad quality use the INLCUDEBAD query modifier as given in the following example.
set starttime='07-05-2011 16:00:00', endtime='07-05-2011 21:00:00' select timestamp,value,quality from ihrawdata where tagname like 'Tag1' and samplingMode=calculated and CalculationMode=count and criteriastring="#INCLUDEBAD" and Numberofsamples=1
Time Stamp Value Quality 7/5/201121:00:00 5.000000000000 100.0000000 Note: When we use INCLUDEBAD query modifier all the values are considered and the count is 5. - Anticipated Usage
-
The INCLUDEBAD modifier can be used to force the Data Archiver to consider every raw sample collected from a field device while still excluding Proficy Historian collection markers or calculation errors and timeouts.
The INCLUDEBAD modifier is usually used if you are writing data with a custom program and not a collector and your program stores meaningful values with bad quality.