Historian in a Cluster Environment
Historian works with the Microsoft Cluster Service Manager to ensure high availability of the Historian server. If the primary Historian node in the cluster experiences difficulties, Historian is automatically started on another node to take over. Server high availability is managed through the Microsoft Cluster Service Manager.
- Read the Important Product Information document and verify that all the prerequisites are properly installed.
- Configure a failover cluster in Windows Server 2008 R2. See Installing Historian in a Cluster Environment. See also Configuring Clusters section in Using Historian Administrator.
- To use Historian Alarms and Events in a cluster environment, select the appropriate SQL Server for both the Cluster Nodes.