Favorites Panel
This area provides access to your stored Favorites list, in alphanumerical order, and access the Favorites Action Menu.
Note: The maximum supported number of Favorites is 100.
Favorites Panel Description
The elements for the Favorites Panel are described in the following table.
Number | Item | Description | |
---|---|---|---|
![]() | Favorites Panel | The Favorites Panel is accessed by clicking the star button in the menu bar. | |
![]() | Unpin/Pin | Pins or unpins the panel in the display to manage space.
The panel is closed when unpinned, but available from the menu. Click Close to close the panel. When closed, click the Favorites to redisplay the view. In either case, the panel drag control remains available to reopen the panel. | |
![]() | Action Menu | Displays the following options:
Refer to Action Menu for more information. | |
![]() | Panel Handle | Lets you drag to increase or decrease the Favorites Panel size. | |
![]() |
| Import/Export Favorites | Allows you to export all your saved favorites as a JSON file that you can import into a different Historian or provide to another user on the same Historian. Note: The maximum supported number of Favorites is 100. |