Alarm and Event Requirements
The following are required to make use of the alarm and event support in Historian:
- An OPC-compliant Alarm & Events Server. This is included with GE Intelligent Platforms products such as CIMPLICITY and iFIX.
- A Microsoft SQL server, such as SQL Server 2008, or SQL Server 2008 express.
- iFIX users must install the iFIXOPC Alarm and Event Server.
- Crystal Reports users must have Crystal Reports 11 or higher installed.
Note: Before starting Alarm Archive service, ensure that "
NT AUTHORITY/SYSTEM
" has "SysAdmin
" privileges.