Calculation Pane Functions
In addition to the VBScript language, there are several built-in functions provided with the Calculation Collector that you can enter in the Calculation Pane. You can type in most of these built-in functions manually or use the wizard to insert them. For a list of the built-in functions, see the Built-In Functions section. For samples, refer to the Examples of Built-In Functions section.
There are two predefined global values called Result and Quality. These global values control the value and quality of the output sample. If the Result is not set in the formula, then no sample is stored.