SET Statements and Variables Examples
Example 1: Perform a Simple SET
If you do not change any variables using the SET
statement or a WHERE
clause in your SELECT
statement, the Historian OLE DB Provider assumes default session variables. For instance, if you do not specify a start and end time for your collected data, the data output from a SELECT
statement would be the last two hours prior to execution of the query.
For example, if you want to SELECT
all of the messages from the ihMessages table for the last day, you would need to explicitly state that you want the messages from the last day in the query. Otherwise, only the messages from the last two hours are displayed when you run the query, since that is what the default assumes.
SET
statement variables persist during a session until changed. You can combine the SET
statement on the same line as the SELECT
statement. The following examples show sample uses of the SET
statement.
SET samplingmode=currentvalue
Example 2: Perform Multiple SETs
SET starttime='14-sep-2001 11:00:00', endtime='14-sep-2001 12:00:00', samplingmode=interpolated, intervalmilliseconds=
Example 3: Prepare for a RawByTime Query
SET starttime='14-sep-2001 11:00:00', endtime='14-sep-2001 12:00:00', samplingmode=rawbytime
Example 4: Prepare for a RawByNumber Query
SET starttime='14-sep-2001 11:00:00', samplingmode=rawbynumber, numberofsamples=10, direction=backward
Example 5: Prepare for One Hour Minimums
SET starttime='15-sep-2001 00:00:00', endtime='16-sep-2001 00:00:00', samplingmode=calculated, intervalmilliseconds=36
Example 6: Prepare for a Filtered Data Query
SET starttime='14-sep-2001 11:00:00', endtime='14-sep-2001 12:00:00', samplingmode=current, filtertag='MY_SERVER.simul
Example 7: Throttle Results with a SET Statement
SET ROWCOUNT = 4
SELECT Tagname FROM ihTags