ihuBrowseCollectors
Prototype
Use the ihuBrowseCollectors
function to browse collectors that are connected to the archiver.
ihuErrorCode IHUAPI ihuBrowseCollectors (
long hServer,
MSO Char *InterfaceNameMask
IHU_COLLECTOR **Collectors,
int *NumOfCollectors
);
Remarks
The inputs to the function are:
hServer
: Server handle for the server to be browsed.*InterfaceNameMask
: Pass*
for all interfaces, or the interface name or detailed mask for efficiency.
The outputs of the function are:
**Collectors
: Returns a list of interfaces/collectors.*NumOfCollectors
: Returns the number of interfaces found.
Returns
The ihuBrowseCollectors
function returns the following values:
ihuSTATUS_OK
ihuSTATUS_FAILED