Chart Editor Descriptions
The elements for the Chart Editor are defined as follows for both charts.
Number | Component | Description |
---|---|---|
![]() | Session Title | Allows you to enter a name for your display session. By default, the title is labeled Click to Add Title until you change it. This will also be the name of your Favorite until you change it. Note: Commas are not permitted in the Title. |
![]() | Chart Title | Allows you to enter a name of that specific chart. The Chart title is automatically labeled Chart 0, Chart 1, Chart 2, and so forth until you change it. |
![]() | Summary Information | Opens up the Summary Information for that chart. This information moves with your cursor. The information that displays includes the following:
|
![]() | Delete |
Deletes the chart without a warning or alert message. Important: When you click Delete, the chart is deleted without a warning message or confirmation prompt.
|
![]() | Legends | Displays the tag name and color for each tag. If all the tags in the chart do not fit in one row of the legend, View All appears on the left side of the screen. Clicking on the right-facing arrow expands the legend above the chart so that all tag names appear with a color depicting their current line color. Hovering your cursor over a tag and clicking the down-arrow to the right of the tag name exposes options for the tag. These options are listed in Chart Editor Options. Clicking on the tag toggles the visibility of the tag in the chart. |
![]() | Statistics | Exposes the raw Historian tag statistics for each tag in the chart. You can sort any column in this table by clicking on a column header or on the up/down arrow in the header. Clicking on the arrow to the left of Statistics toggles the table below the chart. |