Tag Attributes Available when Browsing

While some of these attributes are queried on a browse, they are not shown in the browse interface. These attributes are used when adding a tag, but it is not visible to you whether all attributes come from the server or not.

The following table outlines tag attribute availability when browsing.

Table 1. Tag Attributes
AttributeCapability
Tagname Yes
Source Address Yes
Engineering Unit Description Yes, varies by OPC UA Server vendor.
Data Type Yes. See Recommended Data Types.
Hi Engineering Units Yes, varies by OPC UA Server vendor.
Lo Engineering Units Yes, varies by OPC UA Server vendor.
Is Array Tag Yes
Hi Scale No
Lo Scale No